Current consumption by NVCC_xxx lines if not used (iMX6 Dual core).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current consumption by NVCC_xxx lines if not used (iMX6 Dual core).

461件の閲覧回数
abhijit_mote
Contributor I

What would be the current requirements by all the peripheral supplies (NVCC_xxx) in case if they are not being used?

ラベル(5)
0 件の賞賛
返信
1 返信

391件の閲覧回数
art
NXP Employee
NXP Employee

The current consumption on the I/O supply voltage rails NVCC_xxx depends on the IOMUX pad configuration (e.g. pad function selection, pull-up/down resistors enabling/disabling etc.) even when the corresponding pads are not switching. So, the actual IOUMUX configuration of the corresponding pads should be taken into the account to estimate the currnt consumption on the I/O supply voltage rails.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信