Curious errata# in the schematics of MCIMX6DL-SDP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Curious errata# in the schematics of MCIMX6DL-SDP

ソリューションへジャンプ
1,490件の閲覧回数
torus1000
Contributor V

Hi,

MCIMX6DL-SDB schematic refer to ERR003745 but I couldn't find it in the errata.
   https://www.nxp.com/webapp/Download?colCode=i.MX6_SABRE_SDP_DESIGNFILES
   https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf
But following errata have one.
   https://www.nxp.com/docs/en/errata/IMX6DQCE.pdf

Does ERR003745 for i.MX6D/Q also apply to i.MX6S/DL?

Is it typo of ERR005777(slow starting)?

Can anybody help me?

ERR003745.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,305件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes this is typo and ERR005777 is present in i.MX6SDL errata

https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes this is typo and ERR005777 is present in i.MX6SDL errata

https://www.nxp.com/docs/en/errata/IMX6SDLCE.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信