I have installed Ubuntu 14.04 LTS server edition on a virtual server. I have QT Creator 3.4 installed on a Windows 7 64b machine. My target device is an I.MX287evk equivalent board. Can I cross compile for my arm-linux-generic-elf by simply pointing my cross compiler to the location of the files on the server? Or, is there a way to cross compile with files only installed on the Windows 7 box? I am using Yocto 1.7 (Dizzy) as my BSP.
已解决! 转到解答。
Unfortunately, the toolchain available as part of the Yocto Community BSP is meant to work over Linux. You would need to obtain a toolchain that works over Windows and configure it on QT Creator.
Unfortunately, the toolchain available as part of the Yocto Community BSP is meant to work over Linux. You would need to obtain a toolchain that works over Windows and configure it on QT Creator.