Cross compilation issue with QT5.6 and imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cross compilation issue with QT5.6 and imx6

11,542 Views
pierre_zouz
Contributor I

Hi,

I'm struggling a lot to cross-compile QT-5.6. Did anyone succeed to do it ?

qmake.conf

include(../common/linux_device_pre.conf)

ROOTFS=/mnt/hd

EGLFS_PLATFORM_HOOKS_SOURCES = $$PWD/qeglfshooks_imx6.cpp

QMAKE_LIBS_EGL         += -lEGL

QMAKE_LIBS_OPENGL_ES2  += -lGLESv2 -lEGL -lGAL

QMAKE_LIBS_OPENVG      += -lOpenVG -lEGL -lGAL

IMX6_CFLAGS            = -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1

QMAKE_CFLAGS           += $$IMX6_CFLAGS

QMAKE_CXXFLAGS         += $$IMX6_CFLAGS

QMAKE_LFLAGS           += -Wl,-rpath-link,$$ROOTFS/usr/lib

IMX6_CFLAGS_RELEASE     = -O2 $$IMX6_CFLAGS

QMAKE_CFLAGS_RELEASE   += $$IMX6_CFLAGS_RELEASE

QMAKE_CXXFLAGS_RELEASE += $$IMX6_CFLAGS_RELEASE

QMAKE_CFLAGS_DEBUG     += $$IMX6_CFLAGS

QMAKE_CXXFLAGS_DEBUG   += $$IMX6_CFLAGS

# Preferred eglfs backend

EGLFS_DEVICE_INTEGRATION = eglfs_viv

QMAKE_INCDIR           += $$ROOTFS/usr/include

QMAKE_LIBDIR           += $$ROOTFS/usr/lib

QMAKE_INCDIR_OPENGL_ES2+= $$ROOTFS/usr/include/GLES2

QMAKE_LIBDIR_OPENGL_ES2+= $$ROOTFS/usr/lib

QMAKE_LIBS             += -L/mnt/hd/usr/lib -lgthread-2.0 -lgio-2.0 -lglib-2.0 -lgmodule-2.0 -lgobject-2.0 -lgstbase-0.10 -lgstcontroller-0.10 -lgstreamer-0.10 -lz -lffi -lxml2 -llzma -lm -lmms

include(../common/linux_arm_device_post.conf)

load(qt_config)

My configure settings

export PKG_CONFIG_SYSROOT_DIR=/mnt/hd

export PKG_CONFIG_LIBDIR=/mnt/hd/usr/lib/pkgconfig/

./configure -v -opensource -confirm-license -qt-zlib -no-use-gold-linker -no-reduce-relocations -no-pch -no-xcb -no-opengl -opengl es2 -glib -gstreamer -pkg-config -no-directfb \

-no-cups  -no-dbus -no-icu  -no-android-style-assets -no-sql-db2 -no-sql-ibase -no-sql-mysql -no-sql-oci -no-sql-odbc -no-sql-psql -no-sql-sqlite -no-sql-sqlite2  -no-sql-tds \

-make libs -device imx6 \

-compile-examples \

-device-option CROSS_COMPILE=/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf- \

-sysroot /mnt/hd -no-gcc-sysroot \

-prefix /tmp/qtinstallqt5 \

-skip xmlpatterns -skip winextras -skip webview -skip websockets -skip webengine -skip webchannel -skip wayland -skip serialport -skip serialbus -skip sensors -skip quickcontrols2 -skip multimedia -skip macextras -skip androidextras

                                                                                                         

And errors

[...]

Running configuration tests (phase 1)...

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf-g++ -c -fvisibility=hidden fvisibility.c

Symbol visibility control enabled.

DEFAULT_INCDIRS="/usr/lib64/qt/include

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/include/c++/4.9.2

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/include/c++/4.9.2/arm-linux-gnueabihf

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/include/c++/4.9.2/backward

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/lib/gcc/arm-linux-gnueabihf/4.9.2/include

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/lib/gcc/arm-linux-gnueabihf/4.9.2/include-fixed

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/include

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/libc/usr/include

"

DEFAULT_LIBDIRS="/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/lib

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/libc/lib/arm-linux-gnueabihf

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/libc/lib

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/libc/usr/lib/arm-linux-gnueabihf

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/arm-linux-gnueabihf/libc/usr/lib

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/lib/gcc/arm-linux-gnueabihf/4.9.2

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/lib/gcc/arm-linux-gnueabihf

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/lib/gcc

"

Done running configuration tests.

<srcbase> = /tmp/qt5/qtbase

<outbase> = /tmp/qt5/qtbase

Creating qmake...

gmake: Nothing to be done for `first'.

Running configuration tests (phase 2)...

Found pkg-config from $PATH: /usr/bin/pkg-config

Determining architecture... ()

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp -g -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../mkspecs/devices/linux-imx6-g++ -o arch.o arch.cpp

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -o arch arch.o   -L/mnt/hd/usr/lib -lgthread-2.0 -lgio-2.0 -lglib-2.0 -lgmodule-2.0 -lgobject-2.0 -lgstbase-0.10 -lgstcontroller-0.10 -lgstreamer-0.10 -lz -lffi -lxml2 -llzma -lm -lmms

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/../lib/gcc/arm-linux-gnueabihf/4.9.2/../../../../arm-linux-gnueabihf/bin/ld: skipping incompatible /lib/libc.so.6 when searching for /lib/libc.so.6

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/../lib/gcc/arm-linux-gnueabihf/4.9.2/../../../../arm-linux-gnueabihf/bin/ld: cannot find /lib/libc.so.6

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/../lib/gcc/arm-linux-gnueabihf/4.9.2/../../../../arm-linux-gnueabihf/bin/ld: skipping incompatible /usr/lib/libc_nonshared.a when searching for /usr/lib/libc_nonshared.a

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/../lib/gcc/arm-linux-gnueabihf/4.9.2/../../../../arm-linux-gnueabihf/bin/ld: cannot find /usr/lib/libc_nonshared.a

/tmp/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/../lib/gcc/arm-linux-gnueabihf/4.9.2/../../../../arm-linux-gnueabihf/bin/ld: cannot find /lib/ld-linux.so.3

collect2: error: ld returned 1 exit status

gmake: *** [arch] Error 1

Unable to determine architecture!

[...]

And I got a lot of like this.

Help appreciated :smileyhappy:

Cheers

Tags (1)
0 Kudos
Reply
12 Replies

6,164 Views
gary_bisson
Senior Contributor III

Hi,

I've built it using Buildroot sucessfully. I suggest you do the same, Buildroot will take care of all the dependencies.

It is also possible with Yocto.

Regards,

Gary

0 Kudos
Reply

6,163 Views
pierre_zouz
Contributor I

Hmm...the problem is I already have my system running with a custom 4.4 kernel. I can't simply through away all my environment for an another systems.

All I need is compiling and installing QT5 on imx6. I read a huge numbers of tutorial and forums, I tried a large numbers of cross-compilation tools and methods to build QT5. But it always end with a big fail. So...3 months later...still nothing. So, I have a simple question :

Do it exists a proper up-to-date documentation for compiling natively or cross-compiling QT5 on imx6 ?

Regards,

Pierre

0 Kudos
Reply

6,164 Views
gary_bisson
Senior Contributor III

Hi Pierre,

It's a shame indeed, it never took more than a couple hours with Buildroot to build everything from scratch successfully (kernel/system/Qt5 etc).

How is cross-compiling using buildroot throwing away your environment? It uses its own environment.

Anyway, regardin the documentation, I'm sure you've already been through those since they are the first hits in Google:

I.MX-6 - Qt Wiki

Building QT for i.MX6

As far as I know there isn't much difference between Qt5.5 and Qt5.6 regarding the way it is built.

Then you can have a look at how build system are handling it:

buildroot/qt5base.mk at master · buildroot/buildroot · GitHub

Regards,

Gary

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

Hi Gary,

Thank you for your answers. Unfortunately, I also read these docs and it didn't help. Actually, I would like to know why it's not working my QT5 settings in the first post. I simplified qmake.conf and config.imx6 and I'm still these errors (sorry that's a lot of lines) :

# ./config.imx6                                                                                                                                                                                                                    

This is the Qt Open Source Edition.

You are licensed to use this software under the terms of

the Lesser GNU General Public License (LGPL) versions 2.1.

You are also licensed to use this software under the terms of

the GNU Lesser General Public License (LGPL) versions 3.

You have already accepted the terms of the Open Source license.

Running configuration tests (phase 1)...

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -fvisibility=hidden fvisibility.c

Symbol visibility control enabled.

arm-linux-gnueabi-g++: error: unrecognized command line option '-fuse-ld=gold'

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ --sysroot=/mnt/hd -o libtest.so -shared -Wl,-Bsymbolic-functions -fPIC bsymbolic_functions.c

bsymbolic_functions.c:2:2: error: #error "Symbolic function binding on this architecture may be broken, disabling it (see QTBUG-36129)."

Symbolic function binding disabled.

DEFAULT_INCDIRS="/usr/lib64/qt/include

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/arm-linux-gnueabi/include/c++/4.7.1

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/arm-linux-gnueabi/include/c++/4.7.1/arm-linux-gnueabi

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/arm-linux-gnueabi/include/c++/4.7.1/backward

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/lib/gcc/arm-linux-gnueabi/4.7.1/include

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/lib/gcc/arm-linux-gnueabi/4.7.1/include-fixed

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/arm-linux-gnueabi/include

/mnt/hd/usr/include

"

DEFAULT_LIBDIRS="/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/lib/gcc/arm-linux-gnueabi/4.7.1

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/lib/gcc/arm-linux-gnueabi

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/lib/gcc

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/arm-linux-gnueabi/lib

/mnt/hd/lib

/mnt/hd/usr/lib

"

Done running configuration tests.

Creating qmake...

gmake: Nothing to be done for 'first'.

Running configuration tests (phase 2)...

Found pkg-config from $PATH: /usr/bin/pkg-config

Note: PKG_CONFIG_LIBDIR automatically set to /mnt/hd/usr/lib/pkgconfig:/mnt/hd/usr/share/pkgconfig:/mnt/hd/usr/lib/arm-linux-gnueabi/pkgconfig

Note: PKG_CONFIG_SYSROOT_DIR automatically set to /mnt/hd

Determining architecture... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -g -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../mkspecs/devices/linux-imx6-g++ -o arch.o arch.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -o arch arch.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd

    Found architecture in binary

CFG_ARCH="arm"

CFG_CPUFEATURES=" neon"

Determining architecture... ()

g++ -c -pipe -g -Wall -W -fPIC  -I. -I../../mkspecs/linux-g++ -o arch.o arch.cpp

g++  -o arch arch.o   

    Found architecture in binary

CFG_HOST_ARCH="x86_64"

CFG_HOST_CPUFEATURES=" mmx sse sse2"

System architecture: 'arm'

Host architecture: 'x86_64'

default C++ standard edition auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o c++default.ii -E c++default.cpp

default C++ standard edition enabled.

64-bit std::atomic auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -std=gnu++0x -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o atomic64.o atomic64.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o atomic64 atomic64.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd

64-bit std::atomic enabled.

sse2 auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -msse2 -g -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o sse2.o sse2.cpp

arm-linux-gnueabi-g++: error: unrecognized command line option '-msse2'

Makefile:192: recipe for target 'sse2.o' failed

gmake: *** [sse2.o] Error 1

sse2 disabled.

ipc_sysv auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o ipc.o ipc.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o ipc_sysv ipc.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd

ipc_sysv enabled.

zlib auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o zlib.o zlib.cpp

zlib.cpp: In function 'int main(int, char**)':

zlib.cpp:38:15: warning: variable 'stream' set but not used [-Wunused-but-set-variable]

zlib.cpp:40:17: warning: variable 'ver' set but not used [-Wunused-but-set-variable]

zlib.cpp:43:9: warning: variable 'res' set but not used [-Wunused-but-set-variable]

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o zlib zlib.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lz

zlib enabled.

mtdev auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o mtdev.o mtdev.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o mtdev mtdev.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lmtdev

mtdev enabled.

libjpeg auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o libjpeg.o libjpeg.cpp

libjpeg.cpp:37:21: fatal error: jpeglib.h: No such file or directory

compilation terminated.

Makefile:231: recipe for target 'libjpeg.o' failed

gmake: *** [libjpeg.o] Error 1

libjpeg disabled.

libpng auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o libpng.o libpng.cpp

libpng.cpp: In function 'int main(int, char**)':

libpng.cpp:42:17: warning: variable 'png_ptr' set but not used [-Wunused-but-set-variable]

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o libpng libpng.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lpng

libpng enabled.

libdl auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o libdl.o libdl.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o libdl libdl.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -ldl

libdl enabled.

DB2 auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o db2.o db2.cpp

db2.cpp:34:20: fatal error: sqlcli.h: No such file or directory

compilation terminated.

Makefile:192: recipe for target 'db2.o' failed

gmake: *** [db2.o] Error 1

DB2 disabled.

InterBase auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o ibase.o ibase.cpp

ibase.cpp:34:19: fatal error: ibase.h: No such file or directory

compilation terminated.

Makefile:192: recipe for target 'ibase.o' failed

gmake: *** [ibase.o] Error 1

InterBase disabled.

MySQL (thread-safe) auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/usr/include/mysql -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o mysql.o ../mysql/mysql.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o mysql_r mysql.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -L/usr/lib64 -lpthread -lz -lm -lrt -lssl -lcrypto -ldl -lmysqlclient_r

MySQL (thread-safe) enabled.

OCI auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o oci.o oci.cpp

oci.cpp:34:17: fatal error: oci.h: No such file or directory

compilation terminated.

Makefile:192: recipe for target 'oci.o' failed

gmake: *** [oci.o] Error 1

OCI disabled.

ODBC auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o odbc.o odbc.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o odbc odbc.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lodbc

ODBC enabled.

PostgreSQL auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o psql.o psql.cpp

psql.cpp:34:22: fatal error: libpq-fe.h: No such file or directory

compilation terminated.

Makefile:192: recipe for target 'psql.o' failed

gmake: *** [psql.o] Error 1

PostgreSQL disabled.

SQLite2 auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o sqlite2.o sqlite2.cpp

sqlite2.cpp:34:20: fatal error: sqlite.h: No such file or directory

compilation terminated.

Makefile:192: recipe for target 'sqlite2.o' failed

gmake: *** [sqlite2.o] Error 1

SQLite2 disabled.

TDS auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o tds.o tds.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o tds tds.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lsybdb

TDS enabled.

NIS auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o nis.o nis.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o nis nis.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lnsl

NIS enabled.

Cups auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o cups.o cups.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o cups cups.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lcups

Cups enabled.

POSIX iconv auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o iconv.o iconv.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o iconv iconv.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd

POSIX iconv enabled.

D-Bus auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include/dbus-1.0 -I/mnt/hd/usr/lib64/dbus-1.0/include -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o dbus.o dbus.cpp

In file included from dbus.cpp:35:0:

/mnt/hd/usr/include/dbus-1.0/dbus/dbus.h:29:33: fatal error: dbus/dbus-arch-deps.h: No such file or directory

compilation terminated.

Makefile:208: recipe for target 'dbus.o' failed

gmake: *** [dbus.o] Error 1

D-Bus disabled.

libproxy auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o libproxy.o libproxy.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o libproxy libproxy.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lproxy

libproxy enabled.

Glib auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include/glib-2.0 -I/mnt/hd/usr/lib64/glib-2.0/include -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o glib.o glib.cpp

In file included from /mnt/hd/usr/include/glib-2.0/glib/galloca.h:32:0,

                 from /mnt/hd/usr/include/glib-2.0/glib.h:30,

                 from glib.cpp:36:

/mnt/hd/usr/include/glib-2.0/glib/gtypes.h:32:24: fatal error: glibconfig.h: No such file or directory

compilation terminated.

Makefile:327: recipe for target 'glib.o' failed

gmake: *** [glib.o] Error 1

Glib disabled.

PulseAudio auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -D_REENTRANT -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include/glib-2.0 -I/mnt/hd/usr/lib64/glib-2.0/include -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o pulseaudio.o pulseaudio.cpp

In file included from /mnt/hd/usr/include/glib-2.0/glib/galloca.h:32:0,

                 from /mnt/hd/usr/include/glib-2.0/glib.h:30,

                 from /mnt/hd/usr/include/pulse/glib-mainloop.h:24,

                 from pulseaudio.cpp:35:

/mnt/hd/usr/include/glib-2.0/glib/gtypes.h:32:24: fatal error: glibconfig.h: No such file or directory

compilation terminated.

Makefile:374: recipe for target 'pulseaudio.o' failed

gmake: *** [pulseaudio.o] Error 1

PulseAudio disabled.

OpenGL ES 2.0 auto-detection... ()

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -c -pipe -march=armv7-a -mfpu=neon -DLINUX=1 -DEGL_API_FB=1 -mfloat-abi=softfp --sysroot=/mnt/hd -O2 -Wall -W -fPIC  -I. -I/mnt/hd/usr/include -I../../../mkspecs/devices/linux-imx6-g++ -o opengles2.o opengles2.cpp

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/arm-linux-gnueabi-g++ -Wl,-rpath-link,/mnt/hd/usr/lib -mfloat-abi=softfp -Wl,-O1 -o opengles2 opengles2.o   -L/mnt/hd/usr/lib --sysroot=/mnt/hd -lGLESv2 -lEGL -lGAL

/opt/linaro/gcc-linaro-arm-linux-gnueabi-2012.04-20120426_linux/bin/../lib/gcc/arm-linux-gnueabi/4.7.1/../../../../arm-linux-gnueabi/bin/ld: cannot find -lGAL

collect2: error: ld returned 1 exit status

Makefile:90: recipe for target 'opengles2' failed

gmake: *** [opengles2] Error 1

OpenGL ES 2.0 disabled.

The OpenGL ES 2.0 functionality test failed!

You might need to modify the include and library search paths by editing

QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in

/tmp/qt-everywhere-opensource-src-5.6.1/qtbase/mkspecs/devices/linux-imx6-g++.

Thanks

0 Kudos
Reply

6,164 Views
chenyw
Contributor II

hi! pierre, have you successed?

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

Hi Chen,

Definitely not :smileysad:

0 Kudos
Reply

6,164 Views
chenyw
Contributor II

I'm dealing this with yocto, by replace meta-qt5 layer with new dir git clone from GitHub - meta-qt5/meta-qt5: QT5 layer for openembedded ,but when i run the image,qt demo prompt segmentation fault.

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

Hmmm...is there a doc anywhere about installing meta-qt5 ?

Also, is someone ever built Qt5 natively on imx6 ?

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

Nobody, need to compile QT5 ? Cross-compile ? or Native compilation ?

Bump...

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

bump

0 Kudos
Reply

6,164 Views
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

0 Kudos
Reply

6,164 Views
pierre_zouz
Contributor I

Hi,

Well, I'm not using a specific BSP as I compiled my kernel and packages.

I'm using a 4.4.0 kernel (armv7l Freescale i.MX6 Quad/DualLite ).

Let me know if you need more details.

0 Kudos
Reply