Crontab by Cronie is not working :-(

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Crontab by Cronie is not working :-(

1,126 次查看
fabio_poiatti
Contributor III

I added the cronie lib in local.conf

IMAGE_INSTALL_append+=" cronie"

having now the crontab command available .... but it is not working.

Is there an application note about crontab using? It is not clear the user and the directory ...

For example ...

I'm root user and I have a crontab script already edited ...

1) how can I start the crontab?

2) where I have to put the script with the crontab command?

Thanks

Fabio

0 项奖励
回复
2 回复数

1,058 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello fabio,

Contrab is not in the official repo, you can check this external link to add it:

cronie_1.4.7.bb\cronie\recipes-extended\meta - poky - Poky Build Tool and Metadata 

Regards

0 项奖励
回复

1,058 次查看
fabio_poiatti
Contributor III

ok thanks

0 项奖励
回复