Crontab by Cronie is not working :-(

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Crontab by Cronie is not working :-(

1,157件の閲覧回数
fabio_poiatti
Contributor III

I added the cronie lib in local.conf

IMAGE_INSTALL_append+=" cronie"

having now the crontab command available .... but it is not working.

Is there an application note about crontab using? It is not clear the user and the directory ...

For example ...

I'm root user and I have a crontab script already edited ...

1) how can I start the crontab?

2) where I have to put the script with the crontab command?

Thanks

Fabio

0 件の賞賛
返信
2 返答(返信)

1,089件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello fabio,

Contrab is not in the official repo, you can check this external link to add it:

cronie_1.4.7.bb\cronie\recipes-extended\meta - poky - Poky Build Tool and Metadata 

Regards

0 件の賞賛
返信

1,089件の閲覧回数
fabio_poiatti
Contributor III

ok thanks

0 件の賞賛
返信