Crontab by Cronie is not working :-(

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crontab by Cronie is not working :-(

1,178 Views
fabio_poiatti
Contributor III

I added the cronie lib in local.conf

IMAGE_INSTALL_append+=" cronie"

having now the crontab command available .... but it is not working.

Is there an application note about crontab using? It is not clear the user and the directory ...

For example ...

I'm root user and I have a crontab script already edited ...

1) how can I start the crontab?

2) where I have to put the script with the crontab command?

Thanks

Fabio

0 Kudos
Reply
2 Replies

1,110 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello fabio,

Contrab is not in the official repo, you can check this external link to add it:

cronie_1.4.7.bb\cronie\recipes-extended\meta - poky - Poky Build Tool and Metadata 

Regards

0 Kudos
Reply

1,110 Views
fabio_poiatti
Contributor III

ok thanks

0 Kudos
Reply