Crash log and Kernel dump for ARM architecture with imx6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crash log and Kernel dump for ARM architecture with imx6 processor

2,573 Views
pradeepanbumani
Contributor I

Hi,

I am using device with imx6 processor with

1) linux kernel: 3.18.29

2) openWRT Chaos Calmer.

The issue is, during a kernel panic or crash, no crash logs or the kernel core dump is created. Is there any way to get the logs or the kernel core dump?

In the kernel configuration file, the crash log (CRASHLOG) support is provided only for architectures other than ARM, SPARC, PPC. Is there anyway that we can generate these crash logs for ARM architecture. The dependency to generate crash logs are as below

Symbol: CRASHLOG [=n] 

Type : boolean

Prompt: Crash logging

Location:

(1) -> General setup

Defined at init/Kconfig:1282

Depends on: (!NO_BOOTMEM [=y] || HAVE_MEMBLOCK [=y]) && !ARM [=y] && !SPARC && !PPC

Thanks

0 Kudos
1 Reply

1,306 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pradeep

it is not supported in official linux releases and one can post on OpenWrt wiki:
https://wiki.openwrt.org/doc/hardware/soc/soc.freescale.imx
also may be useful to check

https://community.nxp.com/thread/451773
https://community.nxp.com/docs/DOC-331175

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos