Count of available USB endpoints

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Count of available USB endpoints

Jump to solution
2,494 Views
Mowlwurf
Contributor II

The iMX7D, iMX8M Mini or iMX8M Plus reference manuals state that each USB controller has 8 or 4 programmable bidirectional endpoints (iMX7D: page 3777, iMX8M Mini: page 2653, iMX8M Plus: page 2681)

Does this include the always mandatory control endpoint 0, so only 3 bidirectional endpoints are available for the USB device to function?

Labels (1)
0 Kudos
Reply
1 Solution
2,466 Views
Yuri
NXP Employee
NXP Employee

@Mowlwurf 
Hello,

  Your understanding is correct - this include the always mandatory control endpoint 0.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
2,467 Views
Yuri
NXP Employee
NXP Employee

@Mowlwurf 
Hello,

  Your understanding is correct - this include the always mandatory control endpoint 0.

Regards,
Yuri.

0 Kudos
Reply
2,463 Views
Mowlwurf
Contributor II

Thank you for the clarification.

With that in mind, the 4 endpoints of the iMX8M Plus are not much.
We want to create a compound device that has at least a MTP and a WinUSB interface. Since MTP must have a Bulk-In, a Bulk-Out and an INT-In, that leaves just one bidirectional endpoint for the WinUSB interface.

2,491 Views
kef2
Senior Contributor V
  • bidirectional endpoints

I find this misleading. Vybrid family has "Up to 6 bidirectional endpoints" in reference manual, it has as well DEVEP=6 in read only USB HWDEVICE register. Which really means 6 TX endpoints plus 6 RX endpoints with dedicated bits for each RX and TX endpoints in ENDPTNAK and other registers. So 12 in total. Setup endpoint(s) is included in this count. 

iMX7D has if not the same somewhat similar controller. It has "Up to 8 bidirectional endpoints" in RM, DEVEP=8. This as well means 8 TX endpoints plus 8 RX endpoints. 16 in total.

Can't say about iMX8M, please check reference manual yourself.

Edward