Count of available USB endpoints

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Count of available USB endpoints

跳至解决方案
2,553 次查看
Mowlwurf
Contributor II

The iMX7D, iMX8M Mini or iMX8M Plus reference manuals state that each USB controller has 8 or 4 programmable bidirectional endpoints (iMX7D: page 3777, iMX8M Mini: page 2653, iMX8M Plus: page 2681)

Does this include the always mandatory control endpoint 0, so only 3 bidirectional endpoints are available for the USB device to function?

标签 (1)
0 项奖励
回复
1 解答
2,525 次查看
Yuri
NXP Employee
NXP Employee

@Mowlwurf 
Hello,

  Your understanding is correct - this include the always mandatory control endpoint 0.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,526 次查看
Yuri
NXP Employee
NXP Employee

@Mowlwurf 
Hello,

  Your understanding is correct - this include the always mandatory control endpoint 0.

Regards,
Yuri.

0 项奖励
回复
2,522 次查看
Mowlwurf
Contributor II

Thank you for the clarification.

With that in mind, the 4 endpoints of the iMX8M Plus are not much.
We want to create a compound device that has at least a MTP and a WinUSB interface. Since MTP must have a Bulk-In, a Bulk-Out and an INT-In, that leaves just one bidirectional endpoint for the WinUSB interface.

2,550 次查看
kef2
Senior Contributor V
  • bidirectional endpoints

I find this misleading. Vybrid family has "Up to 6 bidirectional endpoints" in reference manual, it has as well DEVEP=6 in read only USB HWDEVICE register. Which really means 6 TX endpoints plus 6 RX endpoints with dedicated bits for each RX and TX endpoints in ENDPTNAK and other registers. So 12 in total. Setup endpoint(s) is included in this count. 

iMX7D has if not the same somewhat similar controller. It has "Up to 8 bidirectional endpoints" in RM, DEVEP=8. This as well means 8 TX endpoints plus 8 RX endpoints. 16 in total.

Can't say about iMX8M, please check reference manual yourself.

Edward