Could you advice to my i.MX6Q Linux hang issue?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could you advice to my i.MX6Q Linux hang issue?

943 Views
satoshishimoda
Senior Contributor I

Hi community,

 

I created i.MX6Q custom board, but about a half of them hanged when Linux booting.

The attached files are log when it hanged, and we can see the stopping points are different.

Sometimes these can boot correctly, but it will hang rarely.

 

I'm debugging what is wrong, and checking errata, ripple of power supply, clock, DDR calibration with calibration tool in the following URL.

https://community.freescale.com/docs/DOC-94917

But I've not identified the root cause yet.

 

Could you advice me what should I check any other to find the root cause?

And if you can guess what is wrong by the attached log, could you let me know it?

 

Best Regards,

Satoshi Shimoda

Original Attachment has been moved to: mdvr_bootlog.zip

Labels (2)
0 Kudos
6 Replies

546 Views
Yuri
NXP Employee
NXP Employee

What about memory stress test ? Does the system passed it during long time ?

546 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

I tested memory stress test.

Unfortunately, the issue was not resolved even though the board passed the stress test.

So I'm checking power supply, again.

Best Regards,

Satoshi Shimda

0 Kudos

546 Views
YixingKong
Senior Contributor IV

Satoshi

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 Kudos

546 Views
Yuri
NXP Employee
NXP Employee

1.

   Have You checked the design using recent design Checklist recommendations ?

“HW Design Checklist for i.MX6”

https://community.freescale.com/docs/DOC-93819


2.
Is it possible to try JTAG debugging ?


546 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

Thank you for your reply.

OK, I will check the design checklist again and JTAG debugging.

Anyway, I will close this discussion.

I think it is difficult to find the root cause because I have not focus the point I have to check.

So I will create a new discussion when I can narrow down the root cause.

Thank you for your cooperation.

Best Regards,

Satoshi Shimoda

0 Kudos

546 Views
YixingKong
Senior Contributor IV

Satoshi

Thank you for your reply. I will put the discussion in Assumed Answered status. If you have any furhter question late please feel free to come to us.

Thanks,

Yixing

0 Kudos