Could someone help give us a correct DDR4 RPA Excel for Micron DDR4

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Could someone help give us a correct DDR4 RPA Excel for Micron DDR4

180件の閲覧回数
13614278
Contributor III

We are using Micron DDR4 , MT40A2G8, 2 chipset(i.e, totally 4GB DDR4), for IMX8mini

Although we can 'Download' with NXP mscale_ddr_tools_v3.30, but when we click "Calibration", it failed. We doubt our RPA Excel file is not correct.

Could someone give us a correct RPA Excel file for above 'Micron DDR4 , MT40A2G8, 2 chipset(i.e, totally 4GB DDR4),'?

The Excel RPA file we used is attached here, any help would be appreciated, thank you very much!

 

0 件の賞賛
1 返信

172件の閲覧回数
Qmiller
NXP Employee
NXP Employee

You need get correct configs from the MT40A2G8 datasheet.

Qmiller_0-1653013320153.png

 

0 件の賞賛