Could someone help give us a correct DDR4 RPA Excel for Micron DDR4

cancel
Showing results for 
Search instead for 
Did you mean: 

Could someone help give us a correct DDR4 RPA Excel for Micron DDR4

141 Views
13614278
Contributor III

We are using Micron DDR4 , MT40A2G8, 2 chipset(i.e, totally 4GB DDR4), for IMX8mini

Although we can 'Download' with NXP mscale_ddr_tools_v3.30, but when we click "Calibration", it failed. We doubt our RPA Excel file is not correct.

Could someone give us a correct RPA Excel file for above 'Micron DDR4 , MT40A2G8, 2 chipset(i.e, totally 4GB DDR4),'?

The Excel RPA file we used is attached here, any help would be appreciated, thank you very much!

 

0 Kudos
1 Reply

133 Views
Qmiller
NXP Employee
NXP Employee

You need get correct configs from the MT40A2G8 datasheet.

Qmiller_0-1653013320153.png

 

0 Kudos