Could i.MX287 drive the LCD with DE mode control?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could i.MX287 drive the LCD with DE mode control?

454 Views
英库李
Contributor I

Could i.MX287 drive the LCD with DE mode control?

Labels (1)
0 Kudos
1 Reply

329 Views
igorpadykov
NXP Employee
NXP Employee

Hi

yes, programming example where HSYNC and VSYNC signals are not used,

one can find in AN3974 sect.3.4.2.1.2 WVGA Vertical Timing

http://cache.nxp.com/files/dsp/doc/app_note/AN3974.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos