Cortex-M7 is reset when i.MX 8M Plus boots 6.12 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cortex-M7 is reset when i.MX 8M Plus boots 6.12 kernel

357 次查看
JohnE
Contributor II

I am using MCUXpresso SDK 24.12 to run the RPMsg multicore examples on the Cortex-M7 on the i.MX 8M Plus EVK board. These work correctly when run against the default i.MX Linux 5.4 kernel shipped with the EVK board in flash.

I have downloaded the latest i.MX Linux 6.12 kernel prebuilt image from NXP and written the wic image to an SD card.

The A53 boots from the SD card but if I try to run the RPMsg examples I find that the Cortex M7 is reset during the Linux boot sequence. 

I am following the procedure in the i.MX Linux User Guide for v6.12 dated 08 May 25 using the prepare_mcore script and bootaux command to start the Cortex-M7 core before booting Linux on the A53. 

Are these RPMsg examples known to work with the v6.12 kernel on the i.MX 8M Plus EVK?

What might be causing the Cortex-M7 to be reset and is there a fix or workaround?

Thanks,

John

标记 (1)
0 项奖励
回复
1 回复

351 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi @JohnE 

 

We will fix this issue in next SDK version. please use SDK 2.16 instead.

 

Regards

Daniel

0 项奖励
回复