Hi community,
I have some questions about i.MX6 LVDS spec.
Please see my questions as below.
[Q1]
Please see Table 31 in IMX6DQCEC Rev.3.
I want to confirm whether "Differential pulse skew" in this table is same as "Intra-pair skew" which is defined in OpenLDI.
Could you let me know it?
[Q2]
Is there a spec for i.MX6 same as "Inter-pair skew" which is defined in OpenLDI?
If there is no spec for i.MX6, can I understand the skew between differential signal pair is "0"?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi,
yes one can think that skew between differential signal pair is "0".
Best regards
chip
Answers:
1. Yes.
"Differential pulse skew" in Table 31 in IMX6DQCEC Rev.3 is same as "Intra-pair skew" which is defined in OpenLDI
2. No.
Hi chipexpert,
Thank you for your reply.
> 1. Yes.
> "Differential pulse skew" in Table 31 in IMX6DQCEC Rev.3 is same as "Intra-pair skew" which is defined in OpenLDI
OK, I got it.
> 2. No.
I understand the answer is reply to the following question, right?
>"Is there a spec for i.MX6 same as "Inter-pair skew" which is defined in OpenLDI?"
Then, could you give me a comment to the following question also?
>"If there is no spec for i.MX6, can I understand the skew between differential signal pair is "0"?"
Best Regards,
Satoshi Shimoda
Hi Satoshi,
yes one can think that skew between differential signal pair is "0".
Best regards
chip