Correct method to extend DTSI files with conflicting nodes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Correct method to extend DTSI files with conflicting nodes

1,052件の閲覧回数
guilhermes
Contributor II

Hello NXP team,

We're currently designing a hardware board based on the i.MX8QXP-MEK using a different Ethernet PHY controller. To do so, we're currently patching the kernel device tree (imx8x-mek.dtsi) &fec1 node:

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_fec1>;
	phy-mode = "rgmii-txid";
	phy-handle = <&ethphy0>;
	fsl,magic-packet;
	nvmem-cells = <&fec_mac0>;
	nvmem-cell-names = "mac-address";
	rx-internal-delay-ps = <2000>;
	status = "okay";

...


I'd like to include a custom *.dtsi file containing only the new PHY node & its pin definitions, instead of patching the kernel directly - this seems like the better approach.

I believe it is the approach used in a file like the "imx8qxp-mek-ov5640.dtsi", in a way "overriding" the original &fec1 node, and them updating the board's custom yocto machine layer.

Doing so, however, generates a conflict in the DTB compilation, as expected. Is there an example/guide on how to override phandles like the &fec1 in custom *.dtsi files?



0 件の賞賛
返信
1 返信

1,046件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Do you include this dtsi file after #include "imx8qxp-mek.dts"?

Can you share the conflict log in the DTB compilation?

0 件の賞賛
返信