Hello,
Thank you for your comment.
When I took a look at IMX8M Plus Reference Manual, there are three temperature threshold register as below on it.
Immediate temperature threshold : TMHTITR
Average temperature threshold : TMHTATR
Average temperature threhold : TMHTACTR
However, there is no specific definition about the relation of core frequency change and the temperature threshold on IMX8M Plus Reference Manual.
Could you let me know where could I find the description between the temperature and core frequency as followings?
Core Frequency is 1.8GHz : When Temperature range is under xx ℃
Core Frequency is 1.6GHz : When Temperature range is between xx ℃ and xx ℃
Core Frequency is 1.2GHz : When Temperature range is over xx ℃
Best regards
Andy