Copying U-boot from RAM to FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Copying U-boot from RAM to FLASH

ソリューションへジャンプ
3,186件の閲覧回数
vladimirovseych
Contributor III

Hello, Dear Everyone!

Could you explain the way to copy U-Boot, loaded with MFG Tools / Mxsldr into the RAM, to NAND flash?

Thank you very much!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,592件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

MFG Tools / Mxsldr use different appraches, for MFG Tools one

can look at commands in ucl.xml file

Programmers (Flash, etc.) (5)

IMX_MFG_TOOL

http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/switch-monito...

for Mxsldr:

http://www.denx-cs.de/doku/?q=m28evkusbdownloader

http://www.denx.de/wiki/view/DULG/Manual?stickboard=m28evk

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,593件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

MFG Tools / Mxsldr use different appraches, for MFG Tools one

can look at commands in ucl.xml file

Programmers (Flash, etc.) (5)

IMX_MFG_TOOL

http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/switch-monito...

for Mxsldr:

http://www.denx-cs.de/doku/?q=m28evkusbdownloader

http://www.denx.de/wiki/view/DULG/Manual?stickboard=m28evk

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,592件の閲覧回数
vladimirovseych
Contributor III

As I understood it can be made by "nand write ... ". But how can I find out addresses and size of u-boot to copy?

My bootloader size is 3m (0x300000). So what should I write?

nand erase 0x0 0x300000

nand write 0x0 ??? 0x300000

0 件の賞賛
返信