Conversion from Bayer RAW RGB to YUV in IMX6 Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Conversion from Bayer RAW RGB to YUV in IMX6 Solo

5,714 Views
Yogee
Contributor III

Hi,

We need to understand how RAW Bayer 8 bit format from Camera sensor can be converted into YUV422 or anyother format supported by IMX6 solo. There is no YUV output from Camera sensor so this has to be taken care in the IMX6 Solo IPU block. Can anyone advise us on this.

Yogee

Labels (1)
Tags (6)
0 Kudos
Reply
1 Reply

1,036 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yogee

one can use IPU CSC (color space/format convertion), examples

can be found in

IMX51_IPU_LIB_UG

i.MX51 IPU V3 Library User's Guide

Also please check some useful Bayer links below

https://community.freescale.com/message/331888

https://community.freescale.com/message/309833

https://community.freescale.com/message/309069

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply