Control the brightness and contrast of an lvds screen on I.MX6 bord

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Control the brightness and contrast of an lvds screen on I.MX6 bord

3,319 Views
mgk
Contributor I

Hi all,

I would like to control the screen's brightness and contrast on my i.mx6 quad board (an udoo quad board) under ubuntu linaro

I tried to modify the brightness through /sys/class/backlight/pwm-backlight.0/brightness but is not working.

I tried the same thing on other files to do rotation and it worked.

Did someone succeeded to do change these parameters ?

Thanks in advance.

MG

Labels (3)
0 Kudos
Reply
2 Replies

1,894 Views
kane88
Contributor I

echo 200 > /sys/class/backlight/pwm-backlight.0/brightness

try the above & post the status .

does the above help  ???

0 Kudos
Reply

1,894 Views
mgk
Contributor I

Hi,

Thanks for the reply.

I already tried that. No success.

MG

0 Kudos
Reply