Control Register configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Control Register configuration

1,146 次查看
dhanushvenugopa
Contributor I

Hi,

I am using the imx6ul evk board with yocto 4.9.x version ,since i need more number of gpio's I'm tring to mux the ethernet pins ,what value need to be set in the control register, so that the pin gets toggled with the voltage 0 and 3.3v when the  pin is made low and high respectively

标签 (1)
0 项奖励
回复
1 回复

1,063 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dhanush

for i.MX6UL gpio control one can look at

Simple GPIO Example - quandry 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复