Control RS485 Half-Duplex with UART1(ttymxc0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Control RS485 Half-Duplex with UART1(ttymxc0)

1,412件の閲覧回数
peanutstars_job
Contributor II

Hello.

Custom board with imx6dl is based from SABREAUTO RDK board.

I want to control Half-Duplex Mode of RS485 with UART1(ttymxc0).

64.1.1 UART Features  of the datasheet described "RS-485 driver direction control via CTS_B signal".

RS485_Direction Control.PNG

MTXEN485(CTS_B) port set to high when transmit data out, in other case set to low.

Anyway I'm googling this,

normally connect RTS_B to direction control of 485 driver with SER_RS485_ENABLE|SER_RS485_RTS_ON_SEND options.

What is right to connect RS485 driver direction control to CTS_B or RTS_B ?

Thank you.

Regards,

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,234件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi HyunSuk

seems both options can be used, for patches one can look at

[imx6] RS485 could be supported on Imx6 series ?  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信