Hi All,
I have been porting the I2C-HID-CORE feature in iMX8QM-MEK B/D and Android 11.0.0_1_1_0.
I have set up the DTS file (imx8qm-mek.dts).
==============================================
&i2c1_lvds0 {
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lvds0_lpi2c1>;
clock-frequency = <100000>;
status = "okay";
i2c-hid-dev@20 {
compatible = "hid-over-i20";
reg = <0x20>;
hid-descr-addr = <0x0020>;
interrupt-parent = <&lsio_gpio1>;
interrupts =<5 IRQ_TYPE_LEVEL_LOW>;
};
};
================================================
when I set up above the DTS file, our iMX8QM MEK B/B have happened the interrupt continuously.
LVDS0_GPIO01 pin is low active for interrupt.
Please help me to resolve the issue.
Regards
HM
Solved! Go to Solution.
Hi Hyun-mo
for that issue may be recommended to check gpio state with oscilloscope and then debug it
using AN12631 AN12631: Normal and Secure Debug for i.MX8/8X Family of Applications Processors – Application Note
Best regards
igor
Hi Hyun-mo
for that issue may be recommended to check gpio state with oscilloscope and then debug it
using AN12631 AN12631: Normal and Secure Debug for i.MX8/8X Family of Applications Processors – Application Note
Best regards
igor