Console hangs at the moment of i.MX6Q multi-core enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Console hangs at the moment of i.MX6Q multi-core enabled

880件の閲覧回数
torus1000
Contributor V


Hi,

We tried to port L3.14.28 yocto BSP to our custom i.MX6Q board.

Unfortunately kernel boot hung up on the way of enabling 3 other cores.

If 3 of 4 cores disabled with uboot command, it works fine.

What's missing with our settings?

Is there any tips to enable multi-core?

BR

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

809件の閲覧回数
b36401
NXP Employee
NXP Employee

Please make sure that memory map corresponds to your custom board.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信