Console hangs at the moment of i.MX6Q multi-core enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Console hangs at the moment of i.MX6Q multi-core enabled

420 Views
torus1000
Contributor V


Hi,

We tried to port L3.14.28 yocto BSP to our custom i.MX6Q board.

Unfortunately kernel boot hung up on the way of enabling 3 other cores.

If 3 of 4 cores disabled with uboot command, it works fine.

What's missing with our settings?

Is there any tips to enable multi-core?

BR

Labels (3)
Tags (1)
0 Kudos
1 Reply

349 Views
b36401
NXP Employee
NXP Employee

Please make sure that memory map corresponds to your custom board.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos