Connection of Ethernet PHY and i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection of Ethernet PHY and i.MX6

2,537 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about i.MX6 and Ethernet PHY.

Can i.MX6 connect directly to Ethernet PHY ?

I will plan to use a AR8031 in my board because SABRE board is used it.

To use as reference, I have checked two schematics of MCIMX6SX-SDB and SABRE-AVB.

As a result, I found the connection between MCIMX6SX-SDB and SABRE-AVB is a different.

The difference is below:

・MCIMX6SX-SDB has direct connection.

・SABRE-AVB connects via NC7WV16.

Why the SABRE-AVB connects via buffer(NC7WV16) ?

I guess the board needs buffer because it is daughter board type.

Is it correct ?

If not, please tell me the reason.

Furthermore, if you have information, please share me about a distance which is required buffer.

ko-hey

Labels (1)
Tags (3)
4 Replies

1,555 Views
chris321
Contributor IV

the reason for the drivers is noted next to the drivers itself in the schematic:

"Drivers are included in the receive path due to long

signal paths and board-to-board connector. Adopters

should place the PHY and processor on the same board,

and eliminate the drivers. Refer to

Atheros documentation for

additional guidance."

1,555 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thanks, ko-hey, I hadn't checked the schematics for the Atheros ENEY PHY Daughter Board! And thank you chris321 for pointing this note out!

I think this question is answered now.

0 Kudos
Reply

1,555 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ko-hey,

Both the i.MX6 SABRE-SD and the i.MX6 SABRE AI CPU card use the AR8031 with a direct connection. I couldn’t locate the schematic for the SABRE-AVB but in case the i.MX6 and the Ethernet PHY are not in the same board I would say the buffer would make sense. Otherwise it is not required.

0 Kudos
Reply

1,555 Views
ko-hey
Senior Contributor II

Hi gusarambula

Here is schematics. You can get it from "Hardware Development Tools" section. Please check it.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SABRE-AUTO-IMX6-RD2&fpsp=1&tab=Design...

Also please tell me the restriction of length.

ko-hey

0 Kudos
Reply