Connection drops with imx7 picopi wifi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection drops with imx7 picopi wifi

3,849 Views
maash
Contributor II

Hi.

I'm using the meta-avs-demos -yocto project from Codeaurora. I received meta-avs-picopi-wifi from NXP. I've used same bcmdhd drivers in separate form with separately compiled kernel for some time now. And they work pretty badly.

Main issue is the connection drops. In perfect 5GHz network reception the it drops the connection tens of times per day ans sometimes it tries several times before getting connection. Sometimes it might work OK for couple of days.

Interestingly I cannot get connection to some networks at all if I don't have time set correctly. Also the system complains about lack of random numbers. I've tried googling about this for some time now, however there doesn't seem to be fix.

root@imx7d-pico:~# iwconfig wlan0
wlan0 IEEE 802.11abgn ESSID:"xxxxxx"
Mode:Managed Frequency:5.24 GHz Access Point: E0:3F:49:ED:D2:B4
Bit Rate=234 Mb/s Tx-Power=31 dBm
Retry short limit:7 RTS thr:off Fragment thr:off
Encryption key:off
Power Management:on
Link Quality=55/70 Signal level=-55 dBm
Rx invalid nwid:0 Rx invalid crypt:0 Rx invalid frag:0
Tx excessive retries:381 Invalid misc:1 Missed beacon:0

udhcpc (v1.24.1) started
Successfully initialized wpa_supplicant
_dhd_wlfc_mac_entry_update():1649, entry(32)
Sending discover...
Sending discover...
CFG80211-ERROR) wl_cfg80211_connect : Connecting withe0:3f:49:ed:d2:b4 channel (48) ssid "xxxx", len (8)

connect failed event=0 e->status 1 e->reason 0
CFG80211-ERROR) wl_bss_connect_done : Report connect result - connection failed
Sending discover...
CFG80211-ERROR) wl_cfg80211_connect : Connecting withff:ff:ff:ff:ff:ff channel (48) ssid "xxxx", len (8)

CFG80211-ERROR) wl_run_escan : Escan set error (-16)
CFG80211-ERROR) wl_run_escan : error (-16)
CFG80211-ERROR) __wl_cfg80211_scan : Scan err = (-16), busy?-16
CFG80211-ERROR) wl_cfg80211_scan : scan error (-16)
wl_bss_connect_done succeeded with e0:3f:49:ed:d2:b4
wl_bss_connect_done succeeded with e0:3f:49:ed:d2:b4

I'm using haveged to help with the lack of random numbers. However I still occasionally get complain about it.

Any ideas here? I've tried using wext and nl80211.

Labels (3)
0 Kudos
Reply
2 Replies

2,894 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot help you with this problem, this is out of our scope. You will need to go with Technexion, since the problem is with their boards. I apologize for the inconveniences.

Best Regards,

Diego.

0 Kudos
Reply

2,894 Views
maash
Contributor II

This is the log from the actual drop:

root@imx7d-pico:~# CFG80211-ERROR) wl_cfg80211_disconnect : Reason 3

CFG80211-ERROR) wl_is_linkdown : Link down Reason : WLC_E_LINK

link down if wlan0 may call cfg80211_disconnected. event : 16, reason=2 from xx:xx:xx:xx:xx:xx

CFG80211-ERROR) wl_is_linkdown : Link down Reason : WLC_E_DEAUTH

The reason changes between 1, 2 and 3. Mostly tough reason 2 which indicates:

"Client has associated but is not authorised."

(source: https://www.aboutcher.co.uk/2012/07/linux-wifi-deauthenticated-reason-codes/ )

0 Kudos
Reply