Connecting an external card to i2c on imx6sx sabre sd dev board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting an external card to i2c on imx6sx sabre sd dev board

1,146 Views
nurselberlingue
Contributor I

Hi,

I have an i.mx6 solox sabresd dev board. I am trying connect an external  battery pack manager card to through i2c on the dev board. I will have an application which runs on the dev board which interface external battery pack manager.

Looking at the schematic of the dev board all i2c has been assigned and I did not see a pin out like on the imx7 dev board. Where can I connect and how on the imx6 sx sabre sd? Do I need additional h/w? 

What configuration do I need to do to enable r/w it from the user space in linux? I am using buildroot system instead of yocto.

Thank you very much.

0 Kudos
Reply
1 Reply

806 Views
igorpadykov
NXP Employee
NXP Employee

Hi nurselberlinguette 

one can check i2c iomux options for signals which are not used in custom configuration

using Table 4-1. Pin Assignments i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf

Other option use i2c expander, like MAX7310 in Sabre AI schematic sch-27142 (p.17)

Schematics (5)
Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards
Design files for Base Board

SABRE|Automotive-Infotainment|i.MX6|NXP 

For using in linux one can try i2c tools:

https://community.nxp.com/docs/DOC-1477 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply