Connecting a different LVDS panel to the imx53 QSB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting a different LVDS panel to the imx53 QSB

2,764件の閲覧回数
HamsterHunter
Contributor I

Hi,

I need some guidance as to where to do all the changes required to make a different display work.

This is what I have: imx53 QSB with MCIMX-LVDS1 from Freescale, running the Android bsp from Adeneo. This all works fine.

What I want to do: Connect a 10.1 touch panel from "TouchRevolution" to the quick start board.The name of the display is "Fusion 10". It comes with a WSVGA resolution (1024x600). I got all the timing parameters from the manufacturer.

What I did so far:

- I build a custom cable to adapt the display to the board.

- I added the display info to the  file: ../android/i.MX53-QSB-Android-Gingerbread-Release4.2/src/kernel_imx/arch/arm/mach-mx5/mx53_loco.c :

static struct fb_videomode video_modes[] = {
     ...
     {
         .name = "WSVGA",
         .refresh = 60,
         .xres = 1024,
         .yres = 600,
         .pixclock = 48000,
         .left_margin = 104,
         .right_margin = 43,
         .upper_margin = 24,
         .lower_margin = 20,
         .hsync_len = 5,
         .vsync_len = 5,
         .sync = 0,
         .vmode = FB_VMODE_NONINTERLACED,
         .flag = 0,
    },

    ...

}

static struct mxc_fb_platform_data fb_data[] = {
   
              ...
       {
         .interface_pix_fmt = IPU_PIX_FMT_RGB666,
         .mode_str = "WSVGA",
         .mode = video_modes,
        .num_modes = ARRAY_SIZE(video_modes),
       },
       {
        .interface_pix_fmt = IPU_PIX_FMT_LVDS666,
        .mode_str = "WSVGA",
        .mode = video_modes,
        .num_modes = ARRAY_SIZE(video_modes),
      },

            ....
};

- Changed the bootargs to :

   U-Boot> setenv lvds 'setenv bootargs ${bootargs}
   video=mxcdi0fb:RGB666,WSVGA ldb=di0 di0_primary'
   U-Boot> setenv set_display ‘run lvds’
   U-Boot> save

The LCD backlight turns on but the display just stays black. I can't rule out the cable being a problem but I'm rather guessing it's something in the drivers I'm missing.

Can someone please shed some light on to what changes are required to make this work?

Thanks a lot!

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,506件の閲覧回数
yahiaallam
Contributor I

Hey HamsterHunter,

Can you provide more details on how did you build a custom cable to adapt this display to the board?

I've purchased similar one and need to connect it to i.mx6.

0 件の賞賛
返信

1,506件の閲覧回数
HamsterHunter
Contributor I

Thanks! It worked.

I still need to fiddle with the timining parameters though, but that's a different story.  

0 件の賞賛
返信

1,506件の閲覧回数
yvan
Contributor II

Hy,

On the Linux kernel (I think that should be the same for android one), you need to add the _EXACT_ same fb_videomode entry in :

    struct fb_videomode mxcfb_ldb_modedb[]
in file drivers/video/mxc/ldb.c 

0 件の賞賛
返信