Hi,
I need some guidance as to where to do all the changes required to make a different display work.
This is what I have: imx53 QSB with MCIMX-LVDS1 from Freescale, running the Android bsp from Adeneo. This all works fine.
What I want to do: Connect a 10.1 touch panel from "TouchRevolution" to the quick start board.The name of the display is "Fusion 10". It comes with a WSVGA resolution (1024x600). I got all the timing parameters from the manufacturer.
What I did so far:
- I build a custom cable to adapt the display to the board.
- I added the display info to the file: ../android/i.MX53-QSB-Android-Gingerbread-Release4.2/src/kernel_imx/arch/arm/mach-mx5/mx53_loco.c :
static struct fb_videomode video_modes[] = {
...
{
.name = "WSVGA",
.refresh = 60,
.xres = 1024,
.yres = 600,
.pixclock = 48000,
.left_margin = 104,
.right_margin = 43,
.upper_margin = 24,
.lower_margin = 20,
.hsync_len = 5,
.vsync_len = 5,
.sync = 0,
.vmode = FB_VMODE_NONINTERLACED,
.flag = 0,
},
...
}
static struct mxc_fb_platform_data fb_data[] = {
...
{
.interface_pix_fmt = IPU_PIX_FMT_RGB666,
.mode_str = "WSVGA",
.mode = video_modes,
.num_modes = ARRAY_SIZE(video_modes),
},
{
.interface_pix_fmt = IPU_PIX_FMT_LVDS666,
.mode_str = "WSVGA",
.mode = video_modes,
.num_modes = ARRAY_SIZE(video_modes),
},
....
};
- Changed the bootargs to :
U-Boot> setenv lvds 'setenv bootargs ${bootargs}
video=mxcdi0fb:RGB666,WSVGA ldb=di0 di0_primary'
U-Boot> setenv set_display ‘run lvds’
U-Boot> save
The LCD backlight turns on but the display just stays black. I can't rule out the cable being a problem but I'm rather guessing it's something in the drivers I'm missing.
Can someone please shed some light on to what changes are required to make this work?
Thanks a lot!
Hey HamsterHunter,
Can you provide more details on how did you build a custom cable to adapt this display to the board?
I've purchased similar one and need to connect it to i.mx6.
Thanks! It worked.
I still need to fiddle with the timining parameters though, but that's a different story.
Hy,
On the Linux kernel (I think that should be the same for android one), you need to add the _EXACT_ same fb_videomode entry in :
struct fb_videomode mxcfb_ldb_modedb[]
in file drivers/video/mxc/ldb.c