Connecting TI ADC's ASI to NXP's SAI (i2s)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting TI ADC's ASI to NXP's SAI (i2s)

ソリューションへジャンプ
2,517件の閲覧回数
moranmoran
Contributor III

Hello,

It is our first project with audio devices, so I just want to make sure I understand the pinout connection. 

In our project, we are going to use two ADC audio devices on the same bus (TDM) connected to the IMX8 host processor.

If we want to connect the NXP's SAI bus to the audio ADC, should I use SAI_TXC or SAI_RXC? They are both IO, and it is really confusing.

The same question applies to SAI_TXFS and SAI_RXFS.

 

Thanks in advance.

Moran

0 件の賞賛
返信
1 解決策
2,509件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Moran

 

>If we want to connect the NXP's SAI bus to the audio ADC, should I use SAI_TXC or SAI_RXC?

 

SAI_RXC. In particular one can look at Figure 1. I2S/SAI block diagram, it shows transmitter and

receiver sections, AN12090 Using Multi-Channel Feature of SAI

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Moran

 

>If we want to connect the NXP's SAI bus to the audio ADC, should I use SAI_TXC or SAI_RXC?

 

SAI_RXC. In particular one can look at Figure 1. I2S/SAI block diagram, it shows transmitter and

receiver sections, AN12090 Using Multi-Channel Feature of SAI

 

Best regards
igor

0 件の賞賛
返信
2,492件の閲覧回数
moranmoran
Contributor III

Thanks.

0 件の賞賛
返信