I want to access external memory interfaces of imrt1176 in mimxrt1170-evk. To do that I found out that SEMC and flexspi modules can be used. But my doubt is what are the exact peripherals can be accessed through these modules. The biggest doubt is NOR flash. In datasheet it says NOR flash could be accessed via SEMC. But I saw an example code which connects NOR flash via flexspi. I want to clarify this issue.
The next issue is, I coudnt foundout any example codes to access OCT Flash and QSPI flash access via SEMC. Can anyone show me some examples for that.
Final question, is there any internal flash in imxrt1176 chip