Configuring imx6 USB OTG port as USB Host by default

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring imx6 USB OTG port as USB Host by default

5,918 Views
karthigeyannata
Contributor III

We would like to configure imx6 USB OTG port in USB Host mode by default. We have not used USB OTG ID pin in our HW.

Could you please advise the SW changes required to do the same?

Labels (1)
0 Kudos
Reply
2 Replies

1,346 Views
SergioSolis
NXP Employee
NXP Employee


Please take a look at this post and check if it helps you:

IMX53 USB OTG Host mode.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,346 Views
karthigeyannata
Contributor III

After the device is connected when the imx6 is in Host mode,  we would like to do role switch in the software to make imx6 to work in device mode.

is this possible with above mentioned procedure?

0 Kudos
Reply