Configuring i2c for PF1510 on i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring i2c for PF1510 on i.MX6ULL

Jump to solution
1,436 Views
JohnKlug
Senior Contributor I

We are planning on using the PF1510 with the i.MX6ULL processor.  I see this device tree example:

https://github.com/Freescale/linux-fslc/blob/5.4-2.1.x-imx/arch/arm/boot/dts/imx7ulp-evk.dts#L85

 

So for this driver do I not need to specify the i2c address with the i2c controller section of device tree?

0 Kudos
Reply
1 Solution
1,380 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products

Have you seen this patches? Even though they're not in the latest version I think they might be useful for the integration https://community.nxp.com/t5/Power-Management-Knowledge-Base/PMIC-PF1550-i-MX-Processors-Resource/ta....

Thank you for your patience.

Regards

View solution in original post

0 Kudos
Reply
3 Replies
1,381 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products

Have you seen this patches? Even though they're not in the latest version I think they might be useful for the integration https://community.nxp.com/t5/Power-Management-Knowledge-Base/PMIC-PF1550-i-MX-Processors-Resource/ta....

Thank you for your patience.

Regards

0 Kudos
Reply
1,394 Views
JohnKlug
Senior Contributor I

So the driver pf1550-rpmsg.c uses rpmsg, as opposed to the pfuze100.c driver that uses i2c.

rpmsg uses the rpmsg driver, which in turn talks to the mailbox driver?

The mailbox driver is mu, and is only found on certain i.MX processors such as the i.MX7ULP>

 

Is this correct?  So the pf1550-rpmsg.c driver is not compatible with the i.mx6ULL which has no mu hardware feature?

0 Kudos
Reply
1,420 Views
JohnKlug
Senior Contributor I

I think the problem is that the pf1550.c driver is the right driver for i2c, but the source code does not exist in Linux in NXP sources on github. 

The Linux guide for the i.MX family points to:

drivers/regulator/pf1550.c

on page 29 of Rev. LF6.1.1_1.0.0 — 31 March 2023 of the i.MX Linux Reference Manual.

 

Unfortunately in the repository:

regulator directory of Linux

the file pf1550.c does not exist.

And this driver which is present does not use i2c:

rpmsg driver 

I noticed the mcimx6ull-evk kit which runs Linux does not use this part either.

0 Kudos
Reply