Configuring SD card on SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring SD card on SPI

跳至解决方案
1,106 次查看
deepika_t
Contributor IV

Hi Everyone,

We are planning to create a custom i.mx6 board with SD card on SPI. We will be using Android 6 as the Operating system.This SD card will not be used for booting but just for external memory.

Is this  possible? Also what would be the maximum capacity of the SD Card it would support.

If this is possible  then do we have device tree configuration for this.

Thanks and Regards,

Deepika

0 项奖励
回复
1 解答
1,049 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,049 次查看
deepika_t
Contributor IV

Thanks a lot Igor for a quick reply. We need to check for SDIO again

0 项奖励
回复
1,050 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

seems SD card on SPI is not supported as shown on below part of document

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复