Configuring KSZ8795

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring KSZ8795

跳至解决方案
7,528 次查看
aliismail
Contributor IV

Working on a custom board that uses imx6dqscm. We are using the KS8795 switch and having issues with configuring the ethernet. First, we are using the micrel driver, however, it does not seem to support the KS8795 switch. Does anyone know where we can find this driver or a patch? Also, if anyone knows of documentation that can give general guidance to setting up the ethernet?

Thanks!

标签 (3)
0 项奖励
回复
1 解答
5,160 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look at driver at

http://lxr.free-electrons.com/source/drivers/net/phy/spi_ks8995.c
https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Docu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,161 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look at driver at

http://lxr.free-electrons.com/source/drivers/net/phy/spi_ks8995.c
https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Docu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,161 次查看
eric_kang1
Contributor I

Hi Igor,

Long time no see.

I have a question for the RGMII connection between i.MX6Q and KSZ8795 Ethernet Switch.

I have to connect the both via RGMII Interface.

But I couldn't find how to connect the both.

Could you give me any reference schematic for that?

It's very helpful to me if i have that.

Best Regards,

Eric.

0 项奖励
回复
5,161 次查看
stevenguzior
Contributor I

It looks like this driver configures the PHY over SPI.  Is it possible to configure the PHY over MDIO using this driver and binding?

0 项奖励
回复