Configuring CAN Interface at boot up for Android 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Configuring CAN Interface at boot up for Android 10

跳至解决方案
4,041 次查看
tpe
Contributor III

Hello,

My aim is to configure the CAN interface at boot up on a iMX8M device running the Android 10 release. I know that this is normally defined in /etc/network/interfaces for Linux devices and I couldn't find a similar interface file in the Android build. I've attempted to create a service in my init.imx8mq_rc file and wrote a script that executes the CAN interface through the command line.

In my init.imx8mq.rc I have

on property:sys.boot_completed=1
    start init-cancfg-sh

service init-cancfg-sh /vendor/bin/init.cancfg.sh
    class main
    user root
    group root system. 
    oneshot

My script init.cancfg.sh contains

#!/system/bin/sh

ip link set can0 up type can bitrate 250000

Note: I have also set SELinux at boot up time in permissive mode.

The service isn't started and I'm not sure what I'm missing with this approach. I am relatively new to customizing AOSP ROMs and any input would be much appreciated.

Thanks and best regards,

Tony

0 项奖励
回复
1 解答
4,006 次查看
tpe
Contributor III

I solved this issue.

In addition to the setup I had in my description, I had to do the following to get my script to work:

- In device/myvendor/mydevice/sepolicy/file_contexts I added:

    /vendor/bin/init\.cancfg\.sh u:object_r:init-cancfg-sh_exec:s0

- In device/myvendor/mydevice/sepolicy/init-cancfg-sh.te I added a new domain:

    type init-cancfg-sh, domain;
    type init-cancfg-sh_exec, exec_type, vendor_file_type, file_type;

    init_daemon_domain(init-cancfg-sh)

    allow init-cancfg-sh vendor_shell_exec:file rx_file_perms;
    allow init-cancfg-sh vendor_toolbox_exec:file rx_file_perms;

- Copy the script in the device.mk file:

    PRODUCT_COPY_FILES += \
        $(IMX_DEVICE_PATH)/init.cancfg.sh:$(TARGET_COPY_OUT_VENDOR)/bin/init.cancfg.sh

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,250 次查看
Adi99
Contributor I

Hello tony,

I have refer your post and I tried the same script with below content.

#!/system/bin/sh

ip link set can0 up type can bitrate 100000 

if i run same command with adb (ip link set can0 up type can bitrate 100000) it works.

But not work inside the script and init.cancfg.sh throw the error as below.

bitrate not found.

why the same command working on debugg terminal not working inside the sh file.

 

 

 

0 项奖励
回复
4,007 次查看
tpe
Contributor III

I solved this issue.

In addition to the setup I had in my description, I had to do the following to get my script to work:

- In device/myvendor/mydevice/sepolicy/file_contexts I added:

    /vendor/bin/init\.cancfg\.sh u:object_r:init-cancfg-sh_exec:s0

- In device/myvendor/mydevice/sepolicy/init-cancfg-sh.te I added a new domain:

    type init-cancfg-sh, domain;
    type init-cancfg-sh_exec, exec_type, vendor_file_type, file_type;

    init_daemon_domain(init-cancfg-sh)

    allow init-cancfg-sh vendor_shell_exec:file rx_file_perms;
    allow init-cancfg-sh vendor_toolbox_exec:file rx_file_perms;

- Copy the script in the device.mk file:

    PRODUCT_COPY_FILES += \
        $(IMX_DEVICE_PATH)/init.cancfg.sh:$(TARGET_COPY_OUT_VENDOR)/bin/init.cancfg.sh

 

 

0 项奖励
回复