I am using the i.MX 6ULL Applications Processor, seems on this chip , we don't need to use the flexbus to communicate with the oled controller. and we can just configure LCD controller into 8080 to control the SSD1322 controller.
Here is my configuration:
1. Enable the pix-clock bit in CCM regiseter and reset the clock
static void Oled_ControllerReset(void)
{
volatile uint32_t i = 0x100;
/* Disable the clock gate. */
gsOledReg->CTRL_CLR = LCDIF_CTRL_CLKGATE_MASK;
/* Confirm the clock gate is disabled. */
while (gsOledReg->CTRL & LCDIF_CTRL_CLKGATE_MASK);
/* Reset the block. */
gsOledReg->CTRL_SET = LCDIF_CTRL_SFTRST_MASK;
/* Confirm the reset bit is set. */
while (!(gsOledReg->CTRL & LCDIF_CTRL_SFTRST_MASK));
/* Delay for the reset. */
while (i--);
/* Bring the module out of reset. */
gsOledReg->CTRL_CLR = LCDIF_CTRL_SFTRST_MASK;
/* Disable the clock gate. */
gsOledReg->CTRL_CLR = LCDIF_CTRL_CLKGATE_MASK;
}
2. Configure the LCD ctrl register
/* CTRL DATA SELECT CONFIG*/
/* CTRL READ_WRITE SELECT */
/* CTRL BYPASS COUNT SELECT */
/* CTRL BUSY PIN DISABLE*/
gsOledReg->CTRL = (LCDIF_CTRL_READ_WRITEB(0)) | (LCDIF_CTRL_BYPASS_COUNT(0))
|(LCDIF_CTRL_DATA_SELECT(0)) | (LCDIF_CTRL_LCD_DATABUS_WIDTH(0x1U))
|(LCDIF_CTRL_WORD_LENGTH(0x1U)) | (LCDIF_CTRL_MASTER(0x1U))
| (LCDIF_CTRL_RUN_MASK);
/* CTRL1 8080 MODE SELECT */
gsOledReg->CTRL1_CLR = LCDIF_CTRL1_MODE86_MASK;
/* LCD TIMING REGISTER CONFIG*/
gsOledReg->TIMING = LCDIF_TIMING_DATA_SETUP(0x1U) | LCDIF_TIMING_DATA_HOLD(0x1U)
| LCDIF_TIMING_CMD_SETUP(0x1U) | LCDIF_TIMING_CMD_HOLD(0x1U);
3. write data function:
void Oled_WriteData(uint8_t data)
{
/*output cs signal*/
GPIO_WritePinOutput(OLED_CS_GPIO_PORT, OLED_CS_GPIO_PIN, kGPIO_Low);
gsOledReg->CTRL_SET = LCDIF_CTRL_DATA_SELECT_MASK;
/*send data to LCDIF_DATA register*/
gsOledReg->DATA = LCDIF_DATA_DATA_ZERO(data);
/*output cs signal*/
GPIO_WritePinOutput(OLED_CS_GPIO_PORT, OLED_CS_GPIO_PIN, kGPIO_High);
}
However , could anyone check if it is correct?
And I am rather confusing about the description on reference manual. Do we need to set "run" bit and "master" bit in 8080 mode ? what about set the DATA_SHIFT_DIR and SHIFT_NUM_BITS ??