Configure device tree to add sn65dsi83 LVDS bridge on IMX8MQ based platform. Linux 5.15.32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure device tree to add sn65dsi83 LVDS bridge on IMX8MQ based platform. Linux 5.15.32

1,479 Views
bitglitcher
Contributor II

Hello dear IMX support team,

I trying to configure the sn65dsi83 bridge on the device tree of a IMX8MQ based board. I need help understanding what I need to add to the device tree in order to get the sn65dsi83 bridge to work in our product. 

These are some of the errors that I get while booting the board. 

[    1.916423] nwl-dsi 30a00000.mipi-dsi: [drm:nwl_dsi_probe] *ERROR* No valid input endpoint found
[    1.925310] nwl-dsi: probe of 30a00000.mipi-dsi failed with error -22

 

Also can I get directed to some resources regarding the graphical stack of the IMX8MQ processors?

Thanks.

0 Kudos
Reply
0 Replies