Configure and usage of OCRAM for load and run the firmware of M core from imx93 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure and usage of OCRAM for load and run the firmware of M core from imx93 board

239件の閲覧回数
rk4
Contributor I

Hi NXP Team, 

 

Can you explain me exact procedure to use the OCRAM for load and run the firmware (elf file) by remoteproc on M33 core of imx93 board (Digi core connect93).

 

I want OCRAM because the TCM memory has only 128KB available for data and text sections both and I cannot exceed it to 256KB.

 

I want the complete procedure from A core as well M core side to configure OCRAM and run the code larger than the 128KB for our application purpose.

 

Please help me in here. Please ask me if you have any questions regarding this.

 

Thanks

0 件の賞賛
返信
0 返答(返信)