Configure SABRE SD from imx6Quad to imx6Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure SABRE SD from imx6Quad to imx6Dual

Jump to solution
3,440 Views
shu_liu
Contributor II

Hi,

We just started using the MCIMX6Q-SDB evaluation kit. I would like to know how to configure it from imx6Quad to imx6Dual or imx6Solo in software? Thanks.

Regards,

Shu

0 Kudos
Reply
1 Solution
3,305 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shu

dual can be configured with "maxcpus=2" as described in Table 11. Common kernel boot parameters

attached Release Notes. Also for building image one can select appropriate configuration

(for example imx6solosabresd) described in sect.5.1 Build configurations

attached Yocto Guide. Also one can look at sect.5 Enabling Solo Emulation attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,306 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shu

dual can be configured with "maxcpus=2" as described in Table 11. Common kernel boot parameters

attached Release Notes. Also for building image one can select appropriate configuration

(for example imx6solosabresd) described in sect.5.1 Build configurations

attached Yocto Guide. Also one can look at sect.5 Enabling Solo Emulation attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply