Config i.MX6UL OTG2 as OTG mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config i.MX6UL OTG2 as OTG mode?

1,229 Views
viking_yuan
Contributor II
In the default, OTG1 is set as dual mode (OTG) and OTG2 is set as host mode. Is it possible to set OTG2 as dual mode (OTG) and set OTG1 as host mode? If OTG1 is set as host mode, can we still use mfgtools to burn the images via the USB port of OTG1?
0 Kudos
Reply
5 Replies

1,218 Views
igorpadykov
NXP Employee
NXP Employee

Hi viking_yuan

 

>Is it possible to set OTG2 as dual mode (OTG) and set OTG1 as host mode?

 

yes. For example one can look at sect.4.9.9 Changing the Controller Operation Mode

i.MX Linux Reference Manual​

 

>If OTG1 is set as host mode, can we still use mfgtools to burn the images via the USB port of OTG1?

 

not. It should be in device mode for usage with mfgtools.

 

Best regards
igor

0 Kudos
Reply

1,206 Views
viking_yuan
Contributor II

Hi igor,

According to https://community.nxp.com/t5/i-MX-Processors/Configure-USB-OTG2-port-in-peripheral-mode-in-iMX6-Eval... only one of the 2 OTGs can be configured as OTG mode. OTG1 has been configured as OTG mode because of the need to use mfgtools to burn images. So, it means that OTG2 would never be configured as OTG mode because OTG 1 has occupied the OTG setting. Is this correct?

Thanks!

0 Kudos
Reply

1,199 Views
igorpadykov
NXP Employee
NXP Employee

yes correct, according to referenced link with ERR010661, if detach detection is not used

both OTG ports can be used.

 

Best regards
igor

 

0 Kudos
Reply

1,189 Views
viking_yuan
Contributor II

Hi igor,

  What's the setting of OTG 2 if I'd like to set it to OTG mode? I tried the following but it didn't work.

&usbotg2{

        dr_mode = "otg";

        disable-over-current;

        status = "okay";

};

 

0 Kudos
Reply

1,175 Views
viking_yuan
Contributor II

Is there any one who has experienced on setting OTG2 as device mode?

0 Kudos
Reply