Config Tools v26.06

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tools v26.06

245 Views
simonng
Contributor III

Hi NXP,

I upgraded the Config Tools from v25.3 to v25.6.

When I ran the DDR Test, I got the following error. It has no problem if I use v25.3 to run the test. How to solve this problem with the latest v25.6?

Thanks,

Simon

################### Result for: phy_init ###### Run 1 #############################################Microsoft Windows [Version 10.0.26100.4652]

(c) Microsoft Corporation. All rights reserved.

 

C:\nxp\i.MX_CFG_25.06\bin>prompt test-prefix :

 

test-prefix : "C:/nxp/i.MX_CFG_25.06/bin/python3/python" "C:/nxp/i.MX_CFG_25.06/bin/python3/memtool/memtool_entry.py" -t "runtest" -d "C:/ProgramData/NXP/mcu_data_25.06/processors/MIMX9596xxxxN/ksdk2_0/mem_validation/ddrc" -p "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/phy_training_phy_test_0_0_.log" -l INFO "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/connect.json" "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/test.json" "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/phy.json" "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_registers.json" "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_config.json" "C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_config_in.json"

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/connect.json

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/test.json

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/phy.json

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_registers.json

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_config.json

INFO memtool.utils.helper *****C:/Users/eg_fw/AppData/Local/Temp/mem_validation/ddrc_config_in.json

INFO memtool.processor.imx9.imx9_processor Xls mapping load time 0.037542

INFO memtool.processor.imx9.imx9_processor Config time 0.000289

INFO memtool.processor.imx9.imx9_processor DS file time 0.281771

INFO memtool.phyinit.phy_init Run phyinit for 2024.09\lpddr5

INFO memtool.comm.serial_channel Using serial: COM27

ERROR memtool.common.base_test Application load ended with exception: Download incomplete due to configuration error!

0 Kudos
Reply
1 Reply

231 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @simonng 

For the latest Config Tool version 25.06, we only support imx95 chip B0 version, i think your chip is also A1 or A0 version, you need to use the before version tool run the DDR relate test of i.MX95.

B.R

0 Kudos
Reply