ConfigTools for i.MX Version 9.0(i.M6 ULL (MCIMX6Y2XXX08))

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ConfigTools for i.MX Version 9.0(i.M6 ULL (MCIMX6Y2XXX08))

547 Views
ban45
Contributor III

Hi

I used the tool to set up RTS and CTS.
TX and RX are fixed.
Swapping RTS and CTS with the tool did not result in an error.
The RX and TX were able to communicate on the board, but the RTS and CTS signals collided.
Can I change only RTS and CTS like a tool?
It is fixed by the DCE / DTE register.
Is there a way to change only CTS and RTS?
Is there a register that can disable the DCE / DTE register?

Best regrd.

0 Kudos
0 Replies