ConfigTools for i.MX Version 9.0 and MCIMX6Y2CVM08AV pin assignment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ConfigTools for i.MX Version 9.0 and MCIMX6Y2CVM08AV pin assignment

1,048 Views
ban45
Contributor III

Hi,

I set the pin layout with the setting tool.

After setting UART communication TX and RX, I set CTS and RTS.

The error red did not occur when setting CTS and RTS.

Swapping RTS and CTS with the tool did not result in an error.

The RX and TX were able to communicate on the board, but the RTS and CTS signals collided.

(1) Why didn't the tool generate an error?

(2) Can I change only RTS and CTS like a tool?

(3) Does the tool consider DCE / DTE registers?

(4) Is there a register that can invalidate the DCE / DTE register?

・TOOL

Cofig Tools for i.MX6 Version 9.0

・DEVICE

MCIMX6Y2CVM08AV

 

best regard.

0 Kudos
Reply
0 Replies