Concern about i.MX6SL and PF3000 connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Concern about i.MX6SL and PF3000 connection

854 Views
ko-hey
Senior Contributor II

Hi all

 

I have concern about a connection of i.MX6SL and PF3000.

Specifically, connection of POR_B and RESETBMCU.

 

I think the signal's electrical characteristics don't suit each other.

Please give me NXP's opinion.

 

The max VoL of RESETBMCU is 0.4 x OVDD.

On the other hand, the max ViL of POR_B is 0.3 x OVDD.

 

When the PF3000 outputs from 0.3 x OVDD to 0.4 x OVDD, i.MX6SL can't detect it "Low”.

As a result, I guess PF3000 is not suit for i.MX6SL.

 

Q1.

Is above my understanding correct ?

 

Q2.

If Q1 is correct, could you give me the recommendation way to suit the spec ?

 

 

Add info:

I refer following thread too.

https://community.nxp.com/thread/440484

 

The attach is the image which electrical characteristics comes from datasheet.

 

 

Ko-hey

 

Labels (2)
0 Kudos
Reply
3 Replies

709 Views
Yuri
NXP Employee
NXP Employee

Hello,

 The max VoL of RESETBMCU is 0.4 x OVDD for -2mA of load; so,

if load current is smaller, say, because of restriction resistor  the max

VOL should be lower, than 0.4 x OVDD.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

709 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

According to you answer, user need to adjust the voltage by themselves if they choice the PF3000 and i.MX6SL.

Am I correct ?

Ko-hey

0 Kudos
Reply

709 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Yes, it may be needed to apply a restriction resistor for assurance.

Regards,

Yuri.

0 Kudos
Reply