Dear Expert-team,
FEC_EIR[23](MII interrupt) rarely NOT assert when i.MX53 FEC MII data recieve (or read reg of PHY) completed.
If this happend, communication force disconnected. It was clearly not satisfied our product requirements.
Why didn't FEC_EIR[23] flag changed?
Is there any workaround for this?
Thanks.
解決済! 解決策の投稿を見る。
Hi torus1000
one can try to check if this is caused by FEC FIFO overrun issue,
that is FEC DMA cannot access ddr in time:
1, Prioritize the master via M4IF.
Increase FEC priority:
0x63fd_8044=0x33
0x63fd_8048=0x1901a3
2, Increase FEC RX FIFO size.
RX FIFO size = 1.5*(orginal size) => 0x63fe_c150=0x480
RX FIFO size = 1.625*(orginal size) => 0x63fe_c150=0x460
The result as below table, and the patch as below.
Kernel Patch:
--- a/drivers/net/fec.c
+++ b/drivers/net/fec.c
@@ -1300,6 +1300,11 @@ fec_restart(struct net_device *dev, int duplex)
writel(0, fep->hwp + FEC_HASH_TABLE_LOW);
#endif
+ /* Set RX FIFO */
+#ifdef CONFIG_ARCH_MX53
+ writel(0x480, fep->hwp + FEC_R_FSTART);
+#endif
+
/* Set maximum receive buffer size. */
writel(PKT_MAXBLR_SIZE, fep->hwp + FEC_R_BUFF_SIZE);
Uboot patch:
--- a/board/freescale/mx53_smd/lowlevel_init.S
+++ b/board/freescale/mx53_smd/lowlevel_init.S
@@ -81,6 +81,17 @@
beq 1b
.endm
+/* M4IF setup */
+.macro init_m4if
+ ldr r0, =M4IF_BASE_ADDR
+
+ ldr r1, =0x33
+ str r1, [r0, #0x44]
+
+ ldr r1, =0x001901A3
+ str r1, [r0, #0x48]
+.endm /* init_m4if */
+
.macro init_clock
ldr r0, =ROM_SI_REV
ldr r1, [r0]
@@ -218,6 +229,8 @@ lowlevel_init:
init_l2cc
init_aips
+
+ init_m4if
init_clock
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi torus1000
one can try to check if this is caused by FEC FIFO overrun issue,
that is FEC DMA cannot access ddr in time:
1, Prioritize the master via M4IF.
Increase FEC priority:
0x63fd_8044=0x33
0x63fd_8048=0x1901a3
2, Increase FEC RX FIFO size.
RX FIFO size = 1.5*(orginal size) => 0x63fe_c150=0x480
RX FIFO size = 1.625*(orginal size) => 0x63fe_c150=0x460
The result as below table, and the patch as below.
Kernel Patch:
--- a/drivers/net/fec.c
+++ b/drivers/net/fec.c
@@ -1300,6 +1300,11 @@ fec_restart(struct net_device *dev, int duplex)
writel(0, fep->hwp + FEC_HASH_TABLE_LOW);
#endif
+ /* Set RX FIFO */
+#ifdef CONFIG_ARCH_MX53
+ writel(0x480, fep->hwp + FEC_R_FSTART);
+#endif
+
/* Set maximum receive buffer size. */
writel(PKT_MAXBLR_SIZE, fep->hwp + FEC_R_BUFF_SIZE);
Uboot patch:
--- a/board/freescale/mx53_smd/lowlevel_init.S
+++ b/board/freescale/mx53_smd/lowlevel_init.S
@@ -81,6 +81,17 @@
beq 1b
.endm
+/* M4IF setup */
+.macro init_m4if
+ ldr r0, =M4IF_BASE_ADDR
+
+ ldr r1, =0x33
+ str r1, [r0, #0x44]
+
+ ldr r1, =0x001901A3
+ str r1, [r0, #0x48]
+.endm /* init_m4if */
+
.macro init_clock
ldr r0, =ROM_SI_REV
ldr r1, [r0]
@@ -218,6 +229,8 @@ lowlevel_init:
init_l2cc
init_aips
+
+ init_m4if
init_clock
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------