Compiling u-boot-imx after driver update results in fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compiling u-boot-imx after driver update results in fail

1,668 次查看
Clemtos
Contributor I

Hello,

I tried updating the mx6ul_14x14_evk_config/.config file by applying a .bbappend on it and it worked, my driver is going from:

# CONFIG_DRIVER_TI_CPSW is not set
to
CONFIG_DRIVER_TI_CPSW=y

But when I do "bitbake u-boot-imx" I have the following compiling error:

.config:1752:warning: override: reassigning to symbol DRIVER_TI_CPSW

And a bunch of other errors regarding drivers in the log file. I don't know why updating a driver might corrupt the compile process of the u-boot!

See full log file as attached.

 

Thanks

标签 (2)
0 项奖励
回复
2 回复数

1,636 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

I found this record of u-boot modifications in yocto which (in the addendum) seems to correctly override the defconfig, could you try it?

Regards

0 项奖励
回复

1,632 次查看
Clemtos
Contributor I

Hi Joseph,

Unfortunately I already did what this SO is doing by applying a patch  but it was not working.

I created a .bbappend file with the following:

 

FILESEXTRAPATHS:preprend := "${THISDIR}/files:"
SRC_URI:append = " file://u-boot-custom.cfg"

do_configure:append() {
    cat ${WORKDIR}/u-boot-custom.cfg >> ${B}/mx6ul_14x14_evk_config/.config
}

 

 

But when I was running bitbake u-boot-imx I had a compile error:

 

fatal error: asm/arch/cpu.h: No such file or directory
   25 | #include <asm/arch/cpu.h>

 

 

So I manually modified the file to remove the asm/arch in the include to be able to successfully compile. I don't know if my modifications were correct but it compiled the u-boot-imx.

After this I generated a .wic image with the new u-boot and flashed it on my SD Card but I encounter a boot problem:

 

U-Boot 2022.04-lf_v2022.04+g1c881f4da83 (Jun 07 2022 - 05:16:02 +0000)

CPU:   i.MX6ULL rev1.1 900 MHz (running at 396 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 38C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM:  512 MiB
Core:  63 devices, 18 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
        [0] lcdif@21c8000, video
In:    serial
Out:   serial
Err:   serial
data abort
pc : [<9eea1f16>]          lr : [<9eec0b39>]
reloc pc : [<87824f16>]    lr : [<87843b39>]
sp : 9de738a0  ip : 9de7388c     fp : 87800020
r10: 00000017  r9 : 9de7aec0     r8 : 00000100
r7 : 021bc400  r6 : 9eecdb46     r5 : 00000000  r4 : 9de7d9d0
r3 : ffffffff  r2 : 02140000     r1 : 00006cc8  r0 : ffffffff
Flags: NzCv  IRQs off  FIQs off  Mode SVC_32 (T)
Code: 1e03 9300 da0e 6822 (6853) b125
Resetting CPU ...

resetting ...

 

 

Any clue ? Thanks a lot

 

0 项奖励
回复