Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

ソリューションへジャンプ
2,452件の閲覧回数
suehyun_lee
Contributor I

Hi , I am trying to flash image using the UUU tool.

When flashing an image using the UUU tool, can I use "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" in the sample. (I am using sample - L4.19.35_1.1.0_images_MX8MQEVK)

Or should I build "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot"?

If I try to build with below command, some errors occur.

$bitbake fsl-image-mfgtool-initramfs

Errors are about imx-uuc and imx-kobs.

ラベル(2)
1 解決策
2,307件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

元の投稿で解決策を見る

3 返答(返信)
2,308件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

2,307件の閲覧回数
suehyun_lee
Contributor I

Thanks

Using default one, flash succeeded.

0 件の賞賛
返信
2,307件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

OK

0 件の賞賛
返信